Logo
24.12.00
MCUXpresso SDK Project v: latest
Document Release Versions
latest
24.12.00-pvw2
24.12.00

Introduction

  • MCUXpresso SDK
  • Setup

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Examples
  • Middlewares
  • RTOS
  • Boards

Development

  • Architecture
  • Developing with MCUXpresso SDK
  • Build And Configuration System
  • Documentation

Releases

  • Release Notes
mcuxsdk
  • Docs / 24.12.00 »
  • Updating MCU-Link firmware
  • Open on Repo Report an issue with this page

Updating MCU-Link firmware

The LPCXpresso and RW61X hardware platform comes with a CMSIS-DAP-compatible debug interface (known as LPC-Link2). This firmware in this debug interface may be updated using the host computer utility called MCU-Link. This typically used when switching between the default debugger protocol (CMSIS-DAP) to SEGGER J-Link, or for updating this firmware with new releases of these. This section contains the steps to re-program the debug probe firmware.

Note: If MCUXpresso IDE is used and the jumper making DFUlink is installed on the board (JP5 on some boards, but consult the board user manual or schematic for specific jumper number), LPC-Link2 debug probe boots to DFU mode, and MCUXpresso IDE automatically downloads the CMSIS-DAP firmware to the probe before flash memory programming (after clicking Debug). Using DFU mode ensures most up-to-date/compatible firmware is used with MCUXpresso IDE.

NXP provides the MCU-Link utility, which is the recommended tool for programming the latest versions of CMSIS-DAP and J-Link firmware onto FRDM-RW612 or LPCXpresso boards. The utility can be downloaded from https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK.

These steps show how to update the debugger firmware on your board for Windows operating system. For Linux OS, follow the instructions described in the MCU-Link user guide (https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK, select the documentation tab).

  1. Install the MCU-Link utility.

  2. Unplug the board’s USB cable.

  3. Make the DFU link (install the jumper labelled DFUlink, JP10 on FRDM-RW612-BGA board).

  4. Connect the probe to the host via USB (use Link USB connector).

  5. Open a command shell and call the appropriate script located in the MCU-Link installation directory (<MCU-Link install dir>).

    1. To program CMSIS-DAP debug firmware: <LPCScrypt install dir>/scripts/program_CMSIS

    2. To program J-Link debug firmware: <LPCScrypt install dir>/scripts/program_JLINK

  6. Remove DFU link (remove the jumper installed in Step 3).

  7. Re-power the board by removing the USB cable and plugging it in again.

Parent topic:Updating debugger firmware


Copyright 2024, NXP. Last generated on Jan 14, 2025 21:30+0100; branch release/24.12.00, revision 6882aee11e11747f412eb2989d080206781ea9ce.