What is new
The following changes have been implemented compared to the previous SDK release version (24.12.00-pvw2).
Bluetooth LE host stack and applications
Minor fixes and stability improvements
Documentation updates
Bluetooth LE controller
Added initial experimental support for Bluetooth LE Controller feature: Periodic Advertising with Responses (PAwR)\
Minor fixes and stability improvements
Transceiver Drivers (XCVR)
Added API to control PA ramp type and duration
Connectivity framework
Minor Changes (no impact on application)
[Platform]
Ignore the secure bit from RAM addresses when comparing used ram bank in bank retention mechanism
[OTA]
Add choice name to OtaSupport flash selection in Kconfig
[NVM]
Add gNvmErasePartitionWhenFlashing_c feature support to gcc toolchain
[SecLib_RNG]
Misra fixes
Details can be found in CHANGELOG.md
Zigbee and IEEE 802.15.4
Added Zigbee Pro 2023 and examples applications for ZC, ZR, ZED
Introduced experimental support for MAC split architecture with FreeRTOS host stack and examples applications for ZC, ZR, ZED
Fixed PHY low power timer cancellation
Minor fixes for Zigbee PRO R22 configuration
Minor fixes and stability improvements for connectivity_test example application
Fixed the size of TLVs for Node_desc_req in R23 examples
Added experimental Zigbee NCP: coprocessor application and coordinator & router applications for imx8 and x86 platforms