What is new
The following changes have been implemented compared to the previous SDK release version (24.12.00-pvw2).
Bluetooth LE host stack and applications
Minor fixes and stability improvements
Documentation updates
Bluetooth LE controller
Added initial experimental support for Bluetooth LE Controller feature: Periodic Advertising with Responses (PAwR)\
Minor fixes and stability improvements
Transceiver Drivers (XCVR)
Added API to control PA ramp type and duration
Connectivity framework
Minor Changes (no impact on application)
[Platform]
Ignore the secure bit from RAM addresses when comparing used ram bank in bank retention mechanism
[OTA]
Add choice name to OtaSupport flash selection in Kconfig
[NVM]
Add gNvmErasePartitionWhenFlashing_c feature support to gcc toolchain
[SecLib_RNG]
Misra fixes
Details can be found in CHANGELOG.md