What is new

The following changes have been implemented compared to the previous SDK release version (24.12.00-pvw2).

  • Bluetooth LE host stack and applications

    • Minor fixes and stability improvements

    • Documentation updates

  • Bluetooth LE controller

    • Added initial experimental support for Bluetooth LE Controller feature: Periodic Advertising with Responses (PAwR)\

    • Minor fixes and stability improvements

  • Transceiver Drivers (XCVR)

    • Added API to control PA ramp type and duration

  • Connectivity framework

    • Minor Changes (no impact on application)

      • [Platform]

        • Ignore the secure bit from RAM addresses when comparing used ram bank in bank retention mechanism

        • Add gPlatformNbuDebugGpioDAccessEnabled_d Compile Macro (enabled by default). Can be used to disable the NBU debug capability using IOs in case Trustzone is enabled (``PLATFORM_InitNbu()` code executed from unsecure world).

        • Fix in NBU firmware when sending ICS messages gFwkSrvNbuApiRequest_c (from controller_api.h API functions)

      • [OTA]

        • Add choice name to OtaSupport flash selection in Kconfig

      • [NVM]

        • Add gNvmErasePartitionWhenFlashing_c feature support to gcc toolchain

      • [SecLib_RNG]

        • Misra fixes

    Details can be found in CHANGELOG.md