Known issues
The following are the known issues in this release.
Maximum file path length in Windows 7 operating system
The Windows 7 operating system imposes a 260-character maximum length for file paths. When installing the MCUXpresso SDK, place it in a directory close to the root to prevent file paths from exceeding the maximum character length specified by the Windows operating system. The recommended location is the C:\nxp
folder.
Parent topic:Known issues
New project wizard compile failure
The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.
Note: xxx
means core variants, such as, cm0plus
, cm33
, cm4
, cm33_nodsp
.
Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter
and pit_adapter
, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.
Parent topic:Known issues
Only FreeRTOS is tested for RTOS support
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Parent topic:Known issues
Disabled pairing and bonding for most sensor applications
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h
header file.
Parent topic:Known issues
Bluetooth LE
TX data path integrity is not guaranteed during the Bluetooth LE handover, and in some Channel Sounding configurations.
Some instabilities may occur in demanding Bluetooth LE connection scenarios (such as multiple Bluetooth LE connections, very short Connection Intervals).
Bluetooth LE controller:
Max number of connections supported : 8
Potential instabilities particularly with short Connection Intervals
Channel Sounding (CS) not supported:
Mode 3 steps
RTT with Random sequence
RTT Random sequence NADM
Antenna Diversity with CS 1xN / Nx1 (with N >1 and N<=4)
More than one CS procedure in parallel
Note: Documentation may not be fully updated to refer to KW47 devices.
Parent topic:Known issues
Other limitations
Documentation may not be fully updated to refer to KW47 devices.
GenFSK Connectivity_test application is not operational with ARMGCC compiler.
GenFSK
Connectivity_test
application is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
The
--no-warn-rwx-segments
cannot been recognized on legacy MCUXpresso IDE versions.The
--no-warn-rwx-segments
option in MCUXpresso projects should be manually removed from the project settings if someone needs to use legacy (< 11.8.0) MCUXpresso IDE versionsIf the FRO32K is configured as the clock source of Core 0 then the debug session will stuck in both IAR, MCUX CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
In MCUXpresso IDE, the option is in LinkServer Debugger -> Advanced Settings -> Wirespeed (Hz).
If the configuration tool is used to clone
tfm-related
projects, there is a problem that region_defs.h cannot be found in the cloned project.Not supported features:
Platform low power modes not fully enabled in this release.
FRO32K mode not fully supported in this release.
Buttons (SW2/SW3) do not wake up device when it is in low power
Low power reference design applications are not supported for the armgcc toolchain from zip archives. Please use MCUXpresso IDE or IAR toolchains for development using these applications.
Some connection events may be missed by the NBU core firmware when an asynchronous wake up is triggered from the application core.
Parent topic:Known issues
Latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling
The latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling, users need to upgrade to the Linkserver_24.10.22 or higher version, and change the LinkServer path configuration in the MCUX IDE. Two ways to change the LinkerSever path in the MCUX IDE.
Option 1 (recommended): Using the custom Path
Option 2: Using the command-line to change the settings
Close the MCUXpresso IDE if it is open.
Execute the following command:
<path_to_MCUXpressoIDE_installation_folder>\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=<path_to_LinkServer_installation_folder>
where:
<path_to_MCUXpressoIDE_installation_folder>
is the folder where the MCUXpresso IDE is installed.<path_to_LinkServer_installation_folder>
is the folder where the new/custom LinkServer is installed.
Example:
C:\NXP\MCUXpressoIDE_24.9.25\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=c:\NXP\LinkServer_24.10.15
Parent topic:Known issues