What is new
MCUXpresso SDK version 24.12.00 is an early adopter release provided as preview for early development.
The following changes have been implemented compared to the previous SDK release version (24.12.00-pvw2).
Bluetooth LE host stack and applications:
Minor fixes and stability improvements
Documentation updates
Bluetooth LE controller:
Added support for Bluetooth LE Channel Sounding
Minor fixes and stability improvements
Transceiver drivers (XCVR)
Added support for Bluetooth LE Channel Sounding
Added API to control PA ramp type and duration.
Connectivity framework
Minor Changes (no impact on application)
[Platform]
Ignore the secure bit from RAM addresses when comparing used ram bank in bank retention mechanism
Add
gPlatformNbuDebugGpioDAccessEnabled_d
Compile Macro (enabled by default). Can be used to disable the NBU debug capability using IOs in case Trustzone is enabled (``PLATFORM_InitNbu()` code executed from unsecure world).Fix in NBU firmware when sending ICS messages gFwkSrvNbuApiRequest_c (from controller_api.h API functions)
[OTA]
Add choice name to OtaSupport flash selection in Kconfig
[NVM]
Add gNvmErasePartitionWhenFlashing_c feature support to gcc toolchain
[SecLib_RNG]
Misra fixes
Details can be found in CHANGELOG.md