Run a non-XIP (plain load) example application

  1. To debug the application, click the “Start/Stop Debug Session” button, highlighted in red.

    Note: The application is only downloaded into the SRAM when debugging. If you need to program the image to external flash, see Section 4.4, “How to program the non-XIP (plain load) example application to external flash”.

  2. Run the code by clicking the “Run” button to start the application.

    The hello_world application is now running and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.

Parent topic:Run a demo using Keil® MDK/μVision