Install CMSIS device pack
After the MDK tools are installed, Cortex Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions, and flash programming algorithms. Follow these steps to install the RW612 CMSIS pack.
Download the RW612 pack.
After downloading the DFP, double click to install it.
Parent topic:Run a demo using Keil MDK/μVision