MCUXpresso Config Tool support

Steps to generate the project template project for specific derivative part number by MCUXpresso Config Tool:

  1. Download the specific device SDK package and unzip it.

    Note: Since the project template requires FreeMASTER, select the middleware FreeMASTER in the SDK builder when downloading.

  2. Use MCUXpresso Config Tool, See the tool version in the Release Notes document. To create a project template project, as shown in Figure 1.

    |

|

  1. Import the generated template project into CodeWarrior IDE and start the development. By now, a config tool file (extension.mex) with the same project name as shown in Figure 1 is also generated in the project folder. This config tool file achieves easy configurations for pins, clocks, and peripherals.

Parent topic:Project template project for a specific DSC part