Hardware requirements
Micro USB cable
JTAG/SWD debugger
MIMXRT1170-EVKB board
Personal Computer
Speaker with 3.5 mm stereo jack
SD card
Board settings
Please insert the SDCARD into the card slot in order to record to a VoiceSeeker output.
Prepare the Demo
Connect a micro USB cable between the PC host and the debug USB port (J86) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Connect the speaker into the line out jack on MIMXRT1170-EVKB board (J101).
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.