Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
IEE APC Demo started
Erasing Serial NOR over FlexSPI...
Erase data - successfully.
Program data - successfully.
Set up IEE APC regions
Enable IEE APC regions
IEE init
Load keys into IEE
Set up IEE configuration
Load keys into IEE
Set up IEE configuration
Write plain text data to be encrypted at addess 0x20360000:
0x48656c6c6f576f726c64506c61696e21 -> "HelloWorldPlain!"
Turn off ecryption/decryption
Read encrypted data, From address 0x20360000 :
0x26e8146775244a24455d339f45fe098 -> "&ègu$¢DUÓ9ô_à"
Turn on ecryption/decryption
Read decrypted data, From address 0x20360000:
0x48656c6c6f576f726c64506c61696e21 -> "HelloWorldPlain!"
Read decrypted data, From address 0x30014000 (FLASH):
Data are decrypted sucessuly
Turn off ecryption/decryption
Data are encrypted sucessuly
IEE & IEE_APC & Flash demo End.