Hardware requirements
Micro USB cable
MIMXRT1060-EVKC board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Steps to configure the panels
The project uses RK043FN66HS-CT6 panel by default, to use other panels:
If Kconfig is used, select the panel in Kconfig “Panel Selection”.
If package is used, modify the mcux_config.h, change DEMO_PANEL to 0 use RK043FN02H-CT.
Steps to configure the pixel format
The project uses RGB565 pixel format by default.
When Kconfig is used
Select color depth in “Middleware->LVGL Configuration -> Color Settings -> Color depth”, 32-bit, 16-bit, 8-bit are supported.
When package is used
Modify the mcux_config.h change CONFIG_LV_COLOR_DEPTH to 32, 16, 8.
Note:
PXP doesn’t support 8-bit, unselect
LV_USE_PXPin Kconfig, or modify mcux_config.h like:
#define CONFIG_LV_USE_PXP 0
Running the demo
If this example runs correctly, the sample GUI is displayed.