Hardware requirements

  • Mini/micro USB cable

  • EVK_MIMXRT1040 board

  • Personal Computer

Board settings

Connect pin: No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the example in the terminal window:

 Cache example start.

 Cache Invalidate success! 

 Cache Clean success! 
 
 Cache example end.