Hardware requirements
Micro USB cable
MIMXRT1040-EVK board
RK043FN02H-CT or RK043FN66HS-CT6 LCD board
Personal Computer
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK043FN66HS-CT6 by default, to use other panels, change #define DEMO_PANEL DEMO_PANEL_RK043FN66HS to #define DEMO_PANEL DEMO_PANEL_RK043FN02H in emwin_support.h
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Running the demo =============== When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
PXP Rotate example start...