Hardware requirements
Mini/micro USB cable
EVK_MIMXRT1064 board
Personal Computer
Board settings
Connect pin: No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the example in the terminal window:
Cache example start.
Cache Invalidate success!
Cache Clean success!
Cache example end.