Hardware setup
Hardware requirements
MIMXRT1180-EVK RevC
RJ45 Network cable
Mini/micro USB cable
Personal Computer with TwinCAT3
Board settings
For multiple boards cascades, remove the R142 register.
Connection
Connect EtherCAT Port 0 (J28 RJ45 interface) on the MIMXRT1180-EVK board with TwinCAT3 via the Ethernet cable.
Connect a USB cable between the host computer and the OpenSDA USB port on the MIMXRT1180-EVK board.
Open a serial terminal with the following settings.
115,200 baud rate
8 data bits
No parity
One stop bit
No flow control