Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings
This Example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
PFlash Example Start
PFlash Information:
Total Program Flash Size: 512 KB, Hex: (0x80000)
Program Flash Sector Size: 2 KB, Hex: (0x800)
Flash is UNSECURE!
Erase a sector of flash
Successfully Erased Sector 0x7f800 -> 0x80000
Program a buffer to a sector of flash
Successfully Programmed and Verified Location 0x7f800 -> 0x7f810
End of PFlash Example