Hardware requirements
Mini/micro USB cable
FRDM-KE02Z40M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Low Byte test success
High Byte test success
----- Refresh test start -----
----- None-window mode -----
Refresh wdog8 0 time
Refresh wdog8 1 time
Refresh wdog8 2 time
Refresh wdog8 3 time
Refresh wdog8 4 time
Refresh wdog8 5 time
Refresh wdog8 6 time
Refresh wdog8 7 time
Refresh wdog8 8 time
Refresh wdog8 9 time
----- Window mode -----
Refresh wdog8 0 time
Refresh wdog8 1 time
Refresh wdog8 2 time
----- Refresh test success -----
----- End of WDOG8 example -----