Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Low Byte test success
High Byte test success
----- Refresh test start -----
----- None-window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
Refresh wdog32 3 time
Refresh wdog32 4 time
Refresh wdog32 5 time
Refresh wdog32 6 time
Refresh wdog32 7 time
Refresh wdog32 8 time
Refresh wdog32 9 time
----- Window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
----- Refresh test success -----
----- End of WDOG32 example -----