Hardware requirements
Type-C USB cable
FRDM-MCXA166 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the PC host and the MCU-Link USB on the board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, following information can be seen on the MCU-Link terminal:
==FlexCAN loopback functional example -- Start.==
Send message from MB1 to MB0
tx word0 = 0x11223344
tx word1 = 0x55667788
Received message from MB0
rx word0 = 0x11223344
rx word1 = 0x55667788
==FlexCAN loopback functional example -- Finish.==