Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
SPI one board:
Transfer data from instance0 to instance 1 of SPI interface, SPI0 pins are connected with SPI1 pins of board
INSTANCE0 CONNECTS TO INSTANCE1
Pin Name Board Location Pin Name Board Location
MISO J1 pin 11 MISO J2 pin 10
MOSI J1 pin 9 MOSI J2 pin 8
SCK J1 pin 15 SCK J2 pin 12
PCS0 J1 pin 7 PCS0 J2 pin 6
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
SPI one board interrupt example started!
SPI transfer finished!