Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
To measure the frequency or pulse width of external input clock, please connect input clock signal to J9-6(FREQME_GPIO_CLK_A) or J9-5(FREQME_GPIO_CLK_B)
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the freqme_interrupt demo in the terminal window:
FREQME Interrupt Example!
Please select operate mode...
A -- Frequency Measurement Mode.
B -- Pulse Width Measurement Mode.
Frequency Measurement Mode Selected!
Please select the target clock:
A -- XTAL32MHz
B -- FRO_OSC_12M
C -- FREQME_GPIO_CLK_A
D -- FREQME_GPIO_CLK_B
Please input the scale factor of reference clock(Ranges from 0 to 31).
20
Target clock frequency is 11999725 Hz.
Please select operate mode...
A -- Frequency Measurement Mode.
B -- Pulse Width Measurement Mode.