Hardware requirements
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The J8 Pin 28 (ADC0_A2) on EVK board is used to monitor the voltage.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
LPADC Polling Example
ADC Full Range: XXXX
Please press any key to get user channel's ADC value.
ADC value: 2714