Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
To make lpi2c example work, connections needed to be as follows:
LPI2C1 SCL(J2-12) --> LPI2C2 SCL(J2-20)
LPI2C1 SDA(J2-8) --> LPI2C2 SDA(J2-18)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPI2C example -- MasterFunctionalInterrupt_SlaveFunctionalInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
This time , slave will send data:
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
Master received data :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
End of I2C example .