Hardware requirements

  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

Press any key to start example.

Board will enter power deep sleep mode, and then wakeup by OS timer after about 5 seconds.
After Board wakeup, the OS timer will trigger the match interrupt about every 2 seconds.
Board wakeup from deep sleep mode.

OS timer match value reached
OS timer match value reached
OS timer match value reached