Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A
Personal Computer
Board settings
Attach the LCD shield to the FRDM board.
Prepare the Demo
Power the board using a type-c USB cable connected to J2 USB port on the board, attach debugger to J5 connector
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
If this example runs correctly, the sample GUI is displayed.