Hardware requirements

  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the MRT driver demo in the terminal window:

Starting channel No.0 ...
 Channel No.0 interrupt is occured !
 Channel No.0 interrupt is occured !
 Channel No.0 interrupt is occured !

Also the blue led is toggling with interrupt triggering.