Hardware requirements
Micro USB cable
Personal Computer
KW45B41Z-EVK board
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Event task is running.
Receive message counter: 1.
Receive message counter: 2.
Receive message counter: 3.
Receive message counter: 4.
Receive message counter: 5.
Receive message counter: 6.
Receive message counter: 7.
Receive message counter: 8.
Receive message counter: 9.
Receive message counter: 10.
Receive message counter: 11.
Receive message counter: 12.
Event task is running.
Receive message counter: 13.
Receive message counter: 14.