Hardware requirements
Mini/micro USB cable
LPCXpresso51u68 board
Personal Computer
Board settings
Remove jumper for JP9, connect the external input voltage to JP9_2.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the BOD demo in the terminal window:
BOD INTERRUPT EXAMPLE.
Please adjust input voltage low than 3.05V to trigger BOD interrupt.
BOD interrupt occurred, input voltage is low than 3.05V.