Hardware requirements
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings
Insert the card into the card slot
Prepare the Demo
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Card size xxxxx bytes
Working condition:
Voltage : xxxV
Timing mode: xxx
Freq : xxx HZ
Read/Write/Erase the card continuously until encounter error......
Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......
Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.