Hardware requirements
Mini/micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings
(pmux)J11-2(PIO0_0) connect to voltage source1. (nmux)J11-1(PIO0_9) connect to voltage source2.
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP polling driver example
Then change CMP analog input, and the LED GREEN will show the output of the comparator. If the voltage of pmux channel is higher than the voltage of nmux channel, the GREEN LED on the board will be turned on. If the voltage of pmux channel is lower than the voltage of nmux channel, the GREEN LED on the board will be turned off.