Hardware requirements
Micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings
Master_board(SPI7) Slave_board(SPI3)
Pin Name Board Location Pin Name Board Location
MISO J9 pin 11 MISO J12 pin 2
MOSI J9 pin 9 MOSI J12 pin 1
SCK J9 pin 13 SCK J10 pin 16
SSEL0 J12 pin 13 SSEL0 J10 pin 14
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~