Hardware requirements
Two micro USB cables
LPCXpresso55S16 board
Personal Computer
Board settings
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo
Connect a micro USB cable between the host PC and the +5V Power only USB port on the target board (J2).
Connect a micro USB cable between the host PC and the Debug Link USB port on the target board (J1).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the random number generator demo in the terminal window:
Generate 128-bit random number:
0x868516634E5D992656DA94C7BFAD956A
Press any key to continue...