Hardware requirements
Mini/micro USB cable
LPCxpresso55s69 board
Personal Computer
Board settings
Connect a DC voltage source to P19_6 (PIO0_0/CMP IN1)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a macro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP interrupt driver example.
Then change CMP analog input, and the LED GREEN will show the output of the comparator. - Let CMP IN1 voltage be higher than half of the VDDA, LED GREEN on. - Let CMP IN1 voltage be lower than half of the VDDA, LED GREEN off.