Hardware Requirements

  • Mini/micro USB cable

  • LPCXpresso802 board

  • Personal Computer

Board Settings

No special settings are required.

Run the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP port(CN1 on the board).

  2. Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the

    [Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).

  3. Launch the debugger in your IDE to begin running the demo.

Expected Result

When the demo runs successfully, you will find the LED is blinking.