Hardware requirements
2 x Micro USB cable
MC56F81000-EVK board
Personal Computer
Board hardware common setting
Power setting:
Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2
Onboard PnE U-MultiLink debugger setting:
Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.
Board settings
Transfer data from LPI2C0 as master to LPI2C1 as slave
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I2C0_SCL J2-20 I2C1_SCL J3-5
I2C0_SDA J2-18 I2C1_SDA J3-7
Prepare the Demo
Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.
Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with PnE U-MultiLink debug configuration.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPI2C example -- MasterFunctionalInterrupt_SlaveFunctionalInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
This time , slave will send data:
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
Master received data :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
End of I2C example .