Hardware requirements
Mini/micro USB cable
MC56F83000 EVK board
Supported CAN interface (IXXAT, Vector, Kvaser, etc.)
Personal Computer
FreeMASTER 2.5 or later installed on PC
Board settings
CAN transceiver connected to J19 pins
Prepare the Demo
Connect a USB cable between the host PC and the Debug USB port (JM60 USB) on the target board.
Connect CAN transceiver to CAN interface on PC.
Compile and download the program to the target board.
Running the demo
Run FreeMASTER and use connection wizard to connect via FreeMASTER-over-CAN communication plugin at 500kbps.
Click on “FreeMASTER Demonstration Project (embedded in device)” on the Welcome page.
Read more information about FreeMASTER tool at http://www.nxp.com/freemaster.