Hardware requirements

  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

  • headphones with 3.5 mm stereo jack

Board settings

Insert the card into the card slot

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect headphones to Audio HP / Line-Out connector.

  2. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  3. Open a serial terminal with the following settings :

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.