Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
PLU input pins connection:
J20-23 (GPIO4_18) to J1-4 (PLU_IN2).
J20-24 (GPIO4_19) to J1-2 (PLU_IN3).
J20-25 (GPIO4_20) to J1-1 (PLU_IN5).
PLU output pins connection:
J20-17 (PLU_OUT0) to R201(LED_RED).
J20-18 (PLU_OUT1) to R199 (LED_GREEN).
J20-19 (PLU_OUT2) to R200 (LED_BLUE).
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link port(J5 on the board).
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Expected Result
Input source and LED status table:
PLU_IN5 |
PLU_IN4 |
PLU_IN3 |
LED_BLUE |
LED_GREEN |
LED_RED |
---|---|---|---|---|---|
0 |
0 |
0 |
off |
off |
off |
0 |
0 |
1 |
off |
off |
on |
0 |
1 |
0 |
off |
on |
off |
0 |
1 |
1 |
on |
off |
off |
1 |
0 |
0 |
off |
on |
on |
1 |
0 |
1 |
on |
off |
on |
1 |
1 |
0 |
on |
on |
off |
1 |
1 |
1 |
on |
on |
on |
The log below shows the output of the plu combination example in the terminal window:
PLU combination driver example.
Select the input source.
1. Input source 0
2. Input source 1
3. Input source 2
4. Set all three input sources.
0
Select the input value.
0. Low level.
1. High level.
1
Select the input source.
0. Input source 0
1. Input source 1
2. Input source 2
3. Set all three input sources.
3
Input the three values like 000.
0. Low level.
1. High level.
011
The LED will change as the description in the table