Hardware requirements
- Micro USB cable 
- MCX-N5XX-EVK board 
- Personal Computer 
- 3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A 
Board settings
Attach the LCD shield to the EVK board.
Prepare the Demo
- Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board 
- Build the project. 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
If this example runs correctly, the sample GUI is displayed.