Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the GLIKEY driver demo in the terminal window:
GLIKEY Peripheral Driver Example
*Success* GLIKEY is not locked
*Success* GLIKEY Sync Reset done
*Success* GLIKEY Start enable done
*Success* GLIKEY Continue enable Step 1 pass
*Success* GLIKEY Continue enable Step 2 pass
*Success* GLIKEY Continue enable Step 3 pass
*Success* GLIKEY Continue enable Step Enable pass
SUCCESS: Register on index 2 can be now written!
*Success* GLIKEY End of operation done
End of example