Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
USB to serial converter
Board settings
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the DEBUG PORT on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
Lpuart functional interrupt example
Board receives characters then sends them out
Now please input: