Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the terminal displays similar information like the following:
PUFv3 driver example
1510000:TestSelftest:PASS
1510001:TestGenerateRandomData:PASS
1510002:TestEnroll:PASS
1510003:TestStartAfterEnroll:PASS
1510004:TestDeriveDeviceKey:PASS
1510005:TestRandomWrapUnwrap:PASS
1510006:TestUserKeyWrapUnwrap:PASS
1510007:TestStop:PASS
1510008:TestZeroize:PASS
-----------------------
9 Tests 0 Failures 0 Ignored