Hardware requirements

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This example shows two cores communicating using MU. Both M33 and DSP core run at the same time!

When the demo runs successfully, the log would be seen on the M33’s debug terminal like as below and the RED LED is blinking:

MU example polling!
Send: 0. Receive 0
Send: 1. Receive 1
Send: 2. Receive 2
Send: 3. Receive 3
Send: 4. Receive 4
Send: 5. Receive 5
Send: 6. Receive 6
Send: 7. Receive 7
Send: 8. Receive 8
Send: 9. Receive 9
Send: 10. Receive 10
Send: 11. Receive 11
Send: 12. Receive 12
Send: 13. Receive 13
Send: 14. Receive 14
Send: 15. Receive 15
Send: 16. Receive 16
Send: 17. Receive 17
Send: 18. Receive 18
Send: 19. Receive 19
Send: 20. Receive 20
Send: 21. Receive 21
Send: 22. Receive 22
Send: 23. Receive 23
Send: 24. Receive 24
Send: 25. Receive 25
Send: 26. Receive 26
Send: 27. Receive 27
Send: 28. Receive 28
Send: 29. Receive 29
Send: 30. Receive 30
Send: 31. Receive 31
MU example run succeed!