Hardware requirements
Mini USB cable
TWR-KM34Z50MV3 board
Personal Computer
Board settings
Connect J8 1-2 to use potentiometer
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Roll the potentiometer(R20) to change the ADC value. When the demo runs successfully, the following message is displayed in the terminal:
ADC16 interrupt Example.
ADC16_DoAutoCalibration() Done.
Press any key to get user channel's ADC value ...
ADC Value: 1918
ADC Interrupt Count: 1
ADC Value: 1635
ADC Interrupt Count: 2
ADC Value: 1412
ADC Interrupt Count: 3
ADC Value: 1332
ADC Interrupt Count: 4
ADC Value: 1543
ADC Interrupt Count: 5
ADC Value: 1579
ADC Interrupt Count: 6