Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
RTC Example START:
Start Time is 2015/1/21 18:55:30
Ring, ring, ring
Alarm Time is 2015/1/21 18:55:33
RTC Example END.
~~~~~~~~~~~~~~~~~~~~~~~