Hardware requirements
Mini USB cable
TWR-MC56F8200 board
Personal Computer
Oscilloscope
Board hardware common setting
HW reworkd(workaround):
Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings
Connect J501-21 to 3.3V with a 10K resistor. Caution: the 10K resistor must be used in series within J501-21 and 3.3V.
Probe the pwm signal using an oscilloscope
At J501-11
At J501-9
At J501-30
At J501-34
All PWM signals have the same frequency. The J501-11/9 PWM signal is a pair of duty cycle constantly changing complementary signals with a fixed dead time. The J501-30 duty cycle is half of J501-9, and J501-34 duty cycle is half of J501-30.
Connect J501-21 to GND with a 10K resistor. Caution: the 10K resistor must be used in series within J501-21 and GND. Then J501-9/J501-30/J501-34 PWM signals will be disabled.
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
FlexPWM driver example
~~~~~~~~~~~~~~~~~~~~~~~