ecat_foe
Overview
This example demonstrates how to develop EtherCAT FoE(File Access over EtherCAT) example based on Slave Stack Code(SSC).
Note that the demo CAN NOT be built directly. Please see the “Prepare the Demo” section for more details.
Running the demo
When FoE upgrade is successful, the serial port will output:
System reset...
hello sbl.
Bootloader Version 1.9.0
Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1
Secondary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x3
Boot source: none
Swap type: test
Starting swap using move algorithm.
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image
Start the SSC FoE example...
Image version: 2.4.0
Image state: testing
Set image as confirmed: success