camera_view
Overview
This basic example shows how to use the library to create a simple camera preview pipeline. This example also shows how to stop and re-start the pipeline after 3 seconds.
Toolchains supported
MCUXpresso, version 11.10.0
GCC Arm Embedded, version 13.2.Rel1
Hardware requirements
Refer to board.readme for hardware setup requirements.
Pipelines Description
The pipeline created by the application is:
+-------------+ +-------------+ +-------------+
| | | | | |
| camera | --> | 2D convert | --> | Display |
| | | | | |
+-------------+ +-------------+ +-------------+
Camera element is configured for a specific pixel format and resolution (board dependent) Display element is configured for a specific pixel format and resolution (board dependent) 2D convert is configured to perform:
color space conversion from the camera pixel format to the display pixel format
rotation depending on the camera vs display orientation
Running the demo
EXPECTED OUTPUTS: The expected outputs of the example are:
The images captured by the camera should be displayed on the screen