ota_mcuboot_client_wifi
Overview
This application demonstrates an HTTPS OTA client using FreeRTOS + LWIP + MbedTLS + CoreHTTP. The client connects to a HTTPS server and requests an OTA binary for download and subsequent installation by MCUBoot.
Supported Boards
Prepare the Demo
The demo requires MCUBoot bootloader to be present in the FLASH memory to function properly. It is recommended to build and program the bootloader first, then go on with the application. Please refer to respective readme of the mcuboot_opensource example and follow the steps there before you continue.
Go through setup files in the demo source tree
ota_config.handnetwork_cfg.hto check:use of DHCP/static IP
Default HTTPS server IP and port
Default OTA image file path on the server
Before building the example application select Wi-Fi module macro in the
app_config.h. (see#define WIFI_<SoC Name>BOARD<Module Name>). For more information about Wi-Fi module connection see coresponding readme in WiFi examples directory.Connect a USB cable between the PC host and the OpenSDA (or USB to Serial) USB port on the target board.
Open a serial terminal on PC for connected board with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Unix line ending using
\n
Install WiFi connectivity module into SD or M.2 slot if needed.
Running the HTTPS server example
For better experience there is a simple HTTPS server Python3 implementation attached to this example. It was tested with both Windows and Linux, however, it will run on anything supported by Python3.
The directory https_server has the following content:
certs- directory containing a private key and server certificate signed by mbedtls test_ca (found in mbedtls source)httpsd_ota.py- https server code
When run with no parameters it creates a server instance on port 4433:
python3 httpsd_ota.py
With the server code running it is now possible to create connections to this server and request files located in its directory. After the ota image is generated and signed, the last step is to copy it to the server directory.
Running the demo
To get the application properly executed by the bootloader, it is necessary to put signed application image to the primary application partition. There are multiple options how to achieve that, however in principle the are two main methods (both presuming the bootlaoder is already in place):
programing signed application image to the primary application partition using an external tool (direct method)
jump-starting an unsigned application by a debugger, performing OTA update with the signed image, resetting the board and letting the bootloader to perform update (indirect method)
The latter method is described step by step below:
Open the demo project and build it. Known issue: MDK linker issues warning about unused boot_hdr sections. This does not affect the functionality of the example.
Prepare signed image of the application from raw binary as described in the mcuboot_opensource readme.
In case of MCUXpresso raw binary may not be generated automatically. Use binary tools after right clicking Binaries/.axf file in the project tree to generate it manually.
Copy the signed image on your HTTPS server and make sure it’s running. Default image path defined in the client is
/ota.bin.Launch the debugger in your IDE to jump-start the application.
In case of MCUXpresso IDE the execution stalls in an endless loop in the bootloader. Pause the debugging and use debugger console and issue command
jump ResetISR.
When the demo runs successfully, the terminal will display message that coresponds with the following:
OTA HTTPS client demo (WiFi) Initializing WiFi connection... MAC Address: 00:50:43:02:FE:01 Successfully initialized WiFi module Copyright 2022 NXP $
The demo is now waiting for user input. Use
helpto see all available commands.To connect to WiFi network. First use
wifi confcommand to setup network name and password. Thenwifi jointo connect.When connected and with HTTPS server runnning an OTA image is downloaded using
otacommand:$ ota 0 /ota.bin 192.168.1.10 4433
This creates a secure connection to specified server 192.168.1.10 using port 4433 and request file stored at path /ota.bin. The downloaded data will be stored into secondary slot for image 0. Note that it depends on the used platform how many images it uses (see ‘image info’ command for details).
After succesfull download of an OTA image, the command
image infocan be used to inspect the change in the secondary image slot:$ image info Image 0; name APP; state none: Slot 0; slotAddr 8020000; slotSize 655360 <IMAGE APP_PRIMARY: size 373268; version 1.22.0.0> Slot 1; slotAddr 8210000; slotSize 655360 <IMAGE APP_SECONDARY: size 384238; version 2.20.0.0>Now the downloaded image needs to be set as ReadyForTest to inform the bootloader about a new image to be installed and tested upon next reboot:
$ image test 0
This change is reflected in the image state parameter set as ReadyForTest in the
image infocommand output.To trigger installation of new image either reboot the board manually or use
rebootcommand.After new image is installed and booted, again use the
imagecommand to make sure new version of the image is now active and the image state is now set as Testing.Since the image now happens to be in the Testing state, it needs to be accepted with
image acceptcommand:$ image accept 0
This makes sure that upon next reboot the image won’t be reverted to its previous version.